Basic Discrete PAvT
Select the Filter Type from the dropdown list, to set the channel filter of the EXT analyzer; the choices are:
- WIDE (a short Nyquist filter of filter alpha 0.5 and bandwidth 150 kHz).
- NARRow (a short Nyquist filter of filter alpha 0.5 and bandwidth 120 kHz).
- VeryNARrow (a short Nyquist filter of filter alpha 0.5 and bandwidth 80 kHz).
- ExtremelyNARRow (a short Nyquist filter of filter alpha 0.5 and bandwidth 30 kHz).